Everything

R_DACn_Set_ConversionValue

Sets the analog voltage output to the ANOn pin.

 

[Syntax]

#include  “r_cg_macrodriver.h”

void       R_DACn_Set_ConversionValue ( uint8_t reg_value );

Remark         n is the channel number.

 

[Argument(s)]

I/O

Argument

Description

I

Uint8_t reg_value;

D/A conversion value (0x0 to 0xFF)

 

[Return value]

None.