Configures the operation mode of data operation circuit.
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_doc.h”
MD_STATUS R_DOC_SetMode ( doc_mode_t mode, unit16_t value );
[Argument(s)]
I/O |
Argument |
Description |
I |
doc_mode_t mode; |
Operation mode of data operation circuit ADDITION : Data addition mode SUBTRACTION : Data subtraction mode COMPARE_MATCH : Data comparison mode (Detection Condition: Data match is detected) COMPARE_MISMATCH : Data subtraction mode (Detection Condition: Data mismatch is detected) |
I |
uint16_t value; |
Data addition and data subtraction : Results of operations Data comparison : 16-bit data for use as a reference |
[Return value]
Macro |
Description |
MD_OK |
Normal completion |
MD_ARGERROR |
Invalid argument specification |