Everything

r_hofc_interrupt

Performs processing in response to the timer interrupt.

Remark         This API function is called as the interrupt process corresponding to the High-speed on-chip Oscillator clock Frequency Correction function interrupt INTCR.

 

[Syntax]

CA78K0R Compiler

__interrupt static void   r_hofc_interrupt ( void );

 

CC-RL Compiler

static void   _near r_hofc_interrupt ( void );

 

[Argument(s)]

None.

 

[Return value]

None.