Everything

r_iican_callback_master_receiveend

Performs processing in response to the IICA master reception end interrupt INTIICAn.

Remark         This API function is called as the callback routine of interrupt process r_iican_interrupt corresponding to the IICA master reception end interrupt INTIICAn.

 

[Syntax]

static void   r_iican_callback_master_receiveend ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.