Everything

R_WUTM_Set_PowerOff

Halts the clock supplied to the 16-bit wakeup timer.

Remark         Calling this API function changes the 16-bit wakeup timer to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

 

[Syntax]

void       R_WUTM_Set_PowerOff ( void );

 

[Argument(s)]

None.

 

[Return value]

None.