Performs processing in response to the escape transfer end interrupt.
Remark This API function is called as the r_dmac_dmacni_interrupt callback routine, which is generated by escape transfer end.
[Syntax]
static void r_dmacn_callback_transfer_escape_end ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.