Performs processing in response to the exception (other than undefined instruction exception, reset, non-maskable interrupt and unconditional trap).
Remark This API function is called to run interrupt processing for the exceptions other than undefined instruction exception, reset, non-maskable interrupt, and unconditional trap.
[Syntax]
void r_reserved_exception ( void );
[Argument(s)]
None.
[Return value]
None.