Everything

r_rspin_transmit_interrupt

Performs processing in response to the transmit buffer empty interrupts.

Remark         This API function is called to run interrupt processing for the transmit buffer empty interrupts.

 

[Syntax]

static void    r_rspin_transmit_interrupt ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.