Sets the condition for the alarm interrupt (ALM) and allows detection of ALM (binary count mode).
[Syntax]
void R_RTC_Set_BinaryAlarm ( uint32_t alarm_enable, uint32_t alarm_val );
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
uint32_t alarm_enable; |
Comparison flag 0x0 : Comparison does not proceed 0x1 : Comparison proceeds |
|
I |
uint32_t alarm_val; |
The value of the binary counter |
[Return value]
None.