Performs processing in response to the error interrupts.
Remark This API function is called as the r_scifan_erif_interrupt or r_scifan_brif_interrupt callback routine.
[Syntax]
static void r_scifan_callback_error ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.