Everything
20.23 RAM Capacity Estimation
Memory areas used and managed by the RI600PX are broadly classified into four types of sections.
- BRI_RAM section: The RI600PX's management data, data queue area created by the system configuration file, message buffer area created by the system configuration file without specifying section
- RRI_RAM section: The RI600PX's management data (when dynamic creation function is used)
- BURI_HEAP section: Fixed-sized memory pool area and variable-sized memory pool area created by the system configuration file without specifying section
- SURI_STACK section: User stack area of tasks created by the system configuration file without specifying section
- SI section: System stack area
20.23.1 BRI_RAM and RRI_RAM section
The RI600PX's management data is located in the BRI_RAM and RRI_RAM section.
The Table 20-11 shows the size calculation method for the BRI_RAM and RRI_RAM section (unit: bytes). In addition, actual size may become larger than the value computed by Table 20-11 for boundary adjustment.
Table 20-11 BRI_RAM and RRI_RAM Section Size Calculation Method
Object Name
Section
Size Calculation Method (in bytes)
System control block
BRI_RAM
28 + 4×down( ( TMAX_TPRI - 1) / 32 + 1) + TMAX_TPRI
+ VTMAX_SEM + 2×VTMAX_DTQ + VTMAX_FLG + VTMAX_MBX
+ VTMAX_MTX + 2×VTMAX_MBF + VTMAX_MPF + VTMAX_MPL
+ 57×VTMAX_DOMAIN
RRI_RAM1
4 + VTMAX_SEM + 2×VTMAX_DTQ + VTMAX_FLG + VTMAX_MBX
+ VTMAX_MTX + 2×VTMAX_MBF + VTMAX_MPF + VTMAX_MPL
Task control block
BRI_RAM
28×VTMAX_TSK
RRI_RAM2
24×VTMAX_TSK
Semaphore control block3
BRI_RAM
4×VTMAX_SEM + down ( VTMAX_SEM / 8 + 1)
RRI_RAM4
4×VTMAX_SEM
Eventflag control block5
BRI_RAM
8×VTMAX_FLG + 2×down ( VTMAX_FLG / 8 + 1)
RRI_RAM6
4×VTMAX_FLG
Data queue control block7
BRI_RAM
6×VTMAX_DTQ+ down ( VTMAX_DTQ / 8 + 1) + DTQ_ALLSIZE
RRI_RAM8
8×VTMAX_DTQ
Mailbox control block9
BRI_RAM
8×VTMAX_MBX + 2×down ( VTMAX_MBX / 8 + 1)
RRI_RAM10
VTMAX_MBX
Mutex control block11
BRI_RAM
VTMAX_MTX + down ( VTMAX_MTX / 8 + 1)
RRI_RAM12
VTMAX_MTX
Message buffer control block13
BRI_RAM
16×VTMAX_MBF + MBF_ALLSIZE
RRI_RAM14
8×VTMAX_MBF
Fixed-sized memory pool control block15
BRI_RAM
8×VTMAX_MPF + down ( VTMAX_MPF / 8 + 1)
+ (memorypool[].num_block / 8 + 1)
RRI_RAM16
12×VTMAX_MPF
Variable-sized memory pool control block17
BRI_RAM
36×VTMAX_MPL
RRI_RAM18
20×VTMAX_MPL
Cyclic handler control block19
BRI_RAM
8×VTMAX_CYH
RRI_RAM20
20×VTMAX_CYH
Alarm handler control block21
BRI_RAM
8×VTMAX_ALH
RRI_RAM22
8×VTMAX_ALH
2
This area is generated only when Maximum task ID (max_task) is defined.

3
This area is not generated when VTMAX_SEM is 0.

4
This area is generated only when Maximum semaphore ID (max_sem) is defined.

5
This area is not generated when VTMAX_FLG is 0.

6
This area is generated only when Maximum eventflag ID (max_flag) is defined.

7
This area is not generated when VTMAX_DTQ is 0.

8
This area is generated only when Maximum data queue ID (max_dtq) is defined.

9
This area is not generated when VTMAX_MBX is 0.

10
This area is generated only when Maximum mailbox ID (max_mbx) is defined.

11
This area is not generated when VTMAX_MTX is 0.

12
This area is generated only when Maximum mutex ID (max_mtx) is defined.

13
This area is not generated when VTMAX_MBF is 0.

14
This area is generated only when Maximum message buffer ID (max_mbf) is defined.

15
This area is not generated when VTMAX_MPF is 0.

16
This area is generated only when Maximum fixed-sized memory pool ID (max_mpf) is defined.

17
This area is not generated when VTMAX_MPL is 0.

18
This area is generated only when Maximum variable-sized memory pool ID (max_mpl) is defined.

19
This area is not generated when VTMAX_CYH is 0.

20
This area is generated only when Maximum cyclic handler ID (max_cyh) is defined.

21
This area is not generated when VTMAX_ALH is 0.

22
This area is generated only when Maximum alarm handler ID (max_alh) is defined.


Note Each keyword in the size calculation methods has the following meaning.
TMAX_TPRI: The TMAX_TPRI represents maximum task priority.
The cfg600px outputs the macro TMAX_TPRI which defines the value set as Maximum task priority (priority) in System Information (system) to the system information header file kernel_id.h.
VTMAX_TSK: The VTMAX_TSK represents the maximum task ID.
The cfg600px outputs the macro of VTMAX_TSK to the system information header file kernel_id.h. For details, refer to "Maximum task ID (max_task)".
VTMAX_SEM: The VTMAX_SEM represents the maximum semaphore ID.
The cfg600px outputs the macro of VTMAX_SEM to the system information header file kernel_id.h. For details, refer to "Maximum semaphore ID (max_sem)".
VTMAX_FLG: The VTMAX_FLG represents the maximum eventflag ID.
The cfg600px outputs the macro of VTMAX_FLG to the system information header file kernel_id.h. For details, refer to "Maximum eventflag ID (max_flag)".
VTMAX_DTQ: The VTMAX_DTQ represents the maximum data queue ID.
The cfg600px outputs the macro of VTMAX_DTQ to the system information header file kernel_id.h. For details, refer to "Maximum data queue ID (max_dtq)".
DTQ_ALLSIZE: Total of size of data queue area created in the system configuration file. Concretely, it is calculated by the following expressions.
dataqueue[].buffer_size * 4
Note, DTQ_ALLSIZE is 4 when this calculation result is 0.
VTMAX_MBX: The VTMAX_MBX represents the maximum mailbox ID.
The cfg600px outputs the macro of VTMAX_MBX to the system information header file kernel_id.h. For details, refer to "Maximum mailbox ID (max_mbx)".
VTMAX_MTX: The VTMAX_MTX represents the maximum mutex ID.
The cfg600px outputs the macro of VTMAX_MTX to the system information header file kernel_id.h. For details, refer to "Maximum mutex ID (max_mtx)".
VTMAX_MBF: The VTMAX_MBF represents the maximum message buffer ID.
The cfg600px outputs the macro of VTMAX_MBF to the system information header file kernel_id.h. For details, refer to "Maximum message buffer ID (max_mbf)".
MBF_ALLSIZE: Total of size of message buffer area created in the system configuration file without specifying "mbf_section". Concretely, it is calculated by the following expressions.
message_buffer[].mbf_size * 4
VTMAX_MPF: The VTMAX_MPF represents the maximum fixed-sized memory pool ID.
The cfg600px outputs the macro of VTMAX_MPF to the system information header file kernel_id.h. For details, refer to "Maximum fixed-sized memory pool ID (max_mpf)".
VTMAX_MPL: The VTMAX_MPL represents the maximum variable-sized memory pool ID.
The cfg600px outputs the macro of VTMAX_MPL to the system information header file kernel_id.h. For details, refer to "Maximum variable-sized memory pool ID (max_mpl)".
VTMAX_CYH: The VTMAX_CYH represents the maximum cyclic handler ID.
The cfg600px outputs the macro of VTMAX_CYH to the system information header file kernel_id.h. For details, refer to "Maximum cyclic handler ID (max_cyh)".
VTMAX_ALH: The VTMAX_ALH represents the maximum alarm handler ID.
The cfg600px outputs the macro of VTMAX_ALH to the system information header file kernel_id.h. For details, refer to "Maximum alarm handler ID (max_alh)".
VTMAX_DOMAIN: The VTMAX_DOMAIN represents the maximum domain ID.
The cfg600px outputs the macro of VTMAX_DOMAIN to the system information header file kernel_id.h. For details, refer to "Maximum domain ID (max_domain)".
20.23.2 BURI_HEAP section
The fixed-sized memory pool area and variable-sized memory pool area are located in the BURI_HEAP section. Note, when a fixed-sized memory pool and variable-sized memory pool are defined, the area can be located into the user-specific section.
The size of the BURI_HEAP section is calculated by the total of following. In addition, when user specific data is generated in the BURI_HEAP section, the size should be added.
- Total size of fixed-sized memory pool area
This is calculated about the definition of Fixed-sized Memory Pool Information (memorypool[]) that omits to specify "section" by the following expressions.
( memorypool[].siz_block * memorypool[].num_block)
- Total size of variable-sized memory pool area
This is calculated about the definition of Variable-sized Memory Pool Information (variable_memorypool[]) that omits to specify "mpl_section" by the following expressions.
variable_memorypool[].heap_size
20.23.3 SURI_STACK section
The user stack area is located in the SURI_STACK section. Note, when a task is defined, the user stack area can be located into the user-specific section.
The size of the SURI_STACK section is calculated about the definition of Task Information (task[]) that omits to specify "stack_section" by the following expressions. In addition, when user specific data is generated in the SURI_STACK section, the size should be added.
task[].stack_size
Note For estimation of stack size, refer to "APPENDIX D STACK SIZE ESTIMATION".
20.23.4 SI section
The system stack area is located in the SI section.
The system stack size is the same as a set value for System stack size (stack_size) in System Information (system).
Note For estimation of stack size, refer to "APPENDIX D STACK SIZE ESTIMATION".