This option specifies that an object file common to the various devices is generated.
This option is invalid in V2.00.00 or later versions. If this option is specified, it will be ignored but no error will occur due to the compatibility with conventional versions. No warning is output in this case. |
This option does not affect the output code.
When selecting the instruction set to be used, specify the -Xcpu option.