-Xignore_files_misra [Professional Edition only]
|
This option specifies files that will not be checked against the MISRA-C:2004 or MISRA-C:2012 rules.
[Specification format]
-Xignore_files_misra=file[,file]...
|
- | Interpretation when omitted |
All C source files are checked.
[Detailed description]
- | This option does not check the source code of the file specified by file against the MISRA-C:2004 or MISRA-C:2012 rules. |
- | This option is valid only when the -Xmisra2004 or -Xmisra2012 option is specified.
If the -Xmisra2004 or -Xmisra2012 option is not specified, this option will be ignored (A warning will not be output). |
[Example of use]
- | Not to check sample.c against the MISRA-C:2004 rules, describe as: |
>ccrh -Xmisra2004=all -Xignore_files_misra=sample.c -Xcommon=rh850 main.c
|