Everything

 

-change_message [V1.07.00 or later]


This option changes specified warning messages into error messages.

[Specification format]

-change_message=error={num|num1-num2}[, ...]

[Detailed description]

-

This option changes specified warning messages into error messages.

The message numbers that are targeted by this option are W0510000 to W0549999.

-

Specify the rightmost 5 digits of the message number as num, num1, and num2.

If num1-num2 is specified, it is assumed that error numbers within the range have been specified.

-

If num or num1-num2 is omitted, all target warning messages are changed into error messages.

-

When this option is specified more than once, all specifications will be valid.

-

If a message number that does not exist is specified, the specification is ignored.

For message numbers, see "10. MESSAGE".

[Example of use]

-

To change W0520000 to W0549999 into error messages, describe as:

>ccrh -change_message=error=20000-49999 a.c