This option specifies link options.
[Specification format]
- | Interpretation when omitted |
The ccrh driver interprets all specified options.
[Detailed description]
- | This option passes arg to the linker as the link option. |
- | Use this option to pass a file to the linker containing an identifier that the ccrh driver does not recognize as input to the linker. |
- | An error will occur if arg is a non-existent link option. |
- | An error will occur if arg is omitted. |
[Example of use]
- | To pass the -form=relocate option to the linker, describe as: |
>ccrh -Xlk_option=-form=relocate -Xcommon=rh850 main.c
|
The example above has the same meaning as the following.
>ccrh -c -Xcommon=rh850 main.c
>rlink -form=relocate main.obj
|