This option displays the descriptions of asrh options.
[Specification format]
- | Interpretation when omitted |
The descriptions of asrh options are not displayed.
[Detailed description]
- | This option outputs the descriptions of asrh options to the standard error output.
It does not execute assembling. |
[Example of use]
- | To output the descriptions of asrh options to the standard error output, describe as: |