This option enables the PIC facility.
[Specification format]
- | Interpretation when omitted |
The PIC facility is disabled.
[Detailed description]
- | When this option is specified, the relocation attribute that can be specified in the .cseg or .section directive is changed. |
If a relocation attribute shown below is specified, an error will occur.
When this option is specified: TEXT
When this option is not specified: PCTEXT
- | When this option is specified, the predefined macro __PIC will be valid. |
- | If this option is not specified simultaneously with the -pirod option, an error will occur. |
- | This option only controls the relocation attribute that can be specified. The processing for determining whether there is an error in the code for referencing functions is not performed. |