This option specifies information that is output to the list file.
See "3.2 Link Map File" and "3.4 Library List File" for details about output information. |
To output the symbol address, size, type, optimization contents, and number of symbol references, describe as: |
The following table shows whether output information info will be valid or invalid by the combinations of the -form option and the -show or -show=all option. |
If the -rename, -lib_rename, -hide, or -compress option or optimization by deleting unreferenced symbols (-optimize=symbol_delete) is specified, this combination will be invalid. |
The limitations on the output of the cross reference information are shown below.
When optimization is specified during compilation, information about branches to immediate subordinate functions is not output. |