Everything
2.6.4 Relationship with #pragma directives

The behavior of the following options varies depending on the relationship with #pragma directives.

-

When the -Xep=callee or -Xep option is not specified

If the following attribute strings are specified at the same time in a #pragma section, an error will occur.

edata, edata23, tdata, tdata4, tdata5, tdata7, tdata8, ep_auto, ep_disp4, ep_disp5, ep_disp7, ep_disp8, ep_disp16, ep_disp23