Everything

LOW


Returns the low-order 8-bit value of a term.

[Function]

Returns the low-order 8-bit value of a term.

[Application example]

mov     LOW(0xC08), r10        ; (1)

(1)

By executing a mov instruction, this operator returns the low-order 8-bit value "0x8" of the expression "0xC08".
Therefore, (1) in the above example can also be described as: mov 0x8, r10.