Returns the low-order 16-bit value of a term.
[Function]
Returns the low-order 16-bit value of a term.
[Application example]
movea LOWW(0x12345678), R0, r10 ; (1)
|
(1) | By executing a movea instruction, this operator returns the low-order 16-bit value "0x5678" of the expression "0x12345678".
Therefore, (1) in the above example can also be described as: movea 0x5678, R0, r10. |