Everything
5.2.4 Compiler output directives

Compiler output directives inform the assembler of information output by the compiler, such as compiler debugging information.

The following compiler output directives are available.

Table 5.11

Compiler Output Directives

Directive

Overview

.file

Generates a symbol table entry

.line

Line-number information from the C source program

.stack

Defines the stack amount of consumption for a symbol

._line_top

Information specified by the compiler #pragma inline_asm statement

._line_end

Information specified by the compiler #pragma inline_asm statement