The assembler has reserved words. Reserve word cannot be used in symbol, label, section name, macro name. If a reserved word is specified, the CC-RH outputs the message and stops assembling. Reserve word doesn't distinguish between uppercase and lowercase.
The reserved words are as follows.
- | Instructions (such as add, sub, and mov) |
- | Register names, Internal register name |
- | GHS reserved sections ("_GHS", ".ghs", and section names starting with ".__ghs") |