Memory set
[Classification]
Standard library
[Syntax]
#include <string.h>
void *memset(const void *s, int c, size_t length);
[Return value]
Returns the value of s.
[Description]
This function copies the value of c (converted into unsigned char type) to the first length character of an object indicated by s.