Terminates the program
[Classification]
Standard library
[Syntax]
#include <stdlib.h>
void abort(void);
[Description]
Calling abort(void) terminates the program. An abort function that suits the user system must be created in advance.
[Example]
#include <assert.h>
int func(void);
int main() {
int ret;
ret = func();
if (ret == 0) {
abort(); <- abort() is called if ret is not 0
}
return 0;
}
|