Initialization of peripheral devices immediately after the CPU reset.
The peripheral device initialization function performs initialization of peripheral devices immediately after the CPU reset.
This is called from inside the startup routine.
The function included in the library is a dummy routine that performs no actions; code a function in accordance with your system.