The build tool is comprised of components provided by CC-RX. It enables various types of information to be configured via a GUI tool, enabling you to generate load module file or library file from your source files, according to your objectives.
CC-RX is comprised of the four executable files listed below.
(3) rlink: Optimizing linkage editor
Figure 1.1 illustrates the CC-RX processing flow.