Everything
Everything
top
Compiler
Usage Notes
Compatibility with an Older Version or Older Revision
11.5
Compatibility with an Older Version or Older Revision
The effect of the compatibility regarding a version change or revision change is described here.
Differences Information
Previous Topic
Preventing E0562330 Errors in Cases Where Optimization by the Optimizing Linkage Editor is Enabled
Next Topic
V.1.01 and Later Versions (Compatibility with V.1.00)
Table of Contents
Notes on Program Coding
Notes on Compiling a C Program with the C++ Compiler
Notes on Options
Preventing E0562330 Errors in Cases Where Optimization by the Optimizing Linkage Editor is Enabled
Compatibility with an Older Version or Older Revision
V.1.01 and Later Versions (Compatibility with V.1.00)
V.2.00 and Later Versions (Compatibility with Versions between 1.00 and 1.02)
V.2.03 and Later Versions (Compatibility with Versions between 1.00 and 2.02)
V2.06 and Later Versions (Compatibility with V2.05 and earlier)
Version of Compiler Package