2.1 Overview
The resource information tool can be used to confirm and modify the resource information (e.g. system information and memory area information) that changes dynamically as the program executes.
Remarks 1. When a program using the RI850V4 functionality is downloaded, this panel opens automatically.
2. The value will be indeterminate for the resource information shown when the RI850V4 system initialization is incomplete, because it will not be managed by the RI850V4.
2. The quality of the code of the realtime OS is guaranteed and does not need to be analyzed during debugging of user programs. Therefore, the realtime OS resource information displaying plug-in uses the "step-in skip the specified section" facility of the debugger to exclude the OS code from the target of debugging. For details of this step-in facility, see "CS+ RH850 Debug Tool".
On the Realtime OS Resource Information panel tabs (e.g. [System] tab and [Memory Area] tab), check the current status of the resource information.
Change the contents of the resource information (e.g. RI850V4 system time and task status) by issuing service calls from the Realtime OS Resource Information panel.