Everything

1.2 Features

Below are the features of the resource information tool.
- Confirm resource information
When the program running in the debugging tool is stopped at an arbitrary location, the current status of the resource information appears in the Realtime OS Resource Information panel.
- Change resource information
It is possible to dynamically modify the resource information (e.g. the RI850V4 system time and task status) by issuing service calls provided by the RI850V4 from the Realtime OS Resource Information panel.