[Timer Queue] tab |
This tab displays the timer queue information (e.g. Object Type and Number of Objects) of the RI850V4.
This layer displays the timer queue information (e.g. Object Type and Number of Objects) of the RI850V4.
The waiting task information (e.g. Task Name and ID) only appears if there are tasks queued in the timer queue.
Remarks 1. Double-clicking a waiting-task information cell (e.g., Object Name or ID) displays the source file of the task in the Editor panel and moves the caret to the relevant location.
2. Double-clicking the waiting-task information cell for Current Task Stack SP or Task Stack Area displays the contents of the task stack in the Memory panel and moves the caret to the relevant location.
The cyclic handler information (e.g. Cyclic Handler Name and ID) only appears if there are cyclic handlers queued in the timer queue.
Remark Double-clicking a cyclic handler information cell (such as Cyclic Handler Name or ID) displays the source file of the cyclic handler in the Editor panel and moves the caret to the relevant location.
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.