Everything
Everything
top
Debug Tool
FUNCTIONS
2.
FUNCTIONS
This chapter describes a debugging process of CS+ and main functions for debugging.
Differences Information
Previous Topic
Features
Next Topic
Overview
Table of Contents
GENERAL
FUNCTIONS
Overview
Preparation before Debugging
Configuration of Operating Environment of the Debug Tool
Applicable Debugging Methods
Connect to/Disconnect from the Debug Tool
Download/Upload Programs
Display/Change Programs
Usage of PIC/PID Function
Select a Core (PE)
Execute Programs
Stop Programs (Break)
Display/Change the Memory, Register and Variable
Display Information on Function Call from Stack
Collect Execution History of Programs
Measure Execution Time of Programs
Measure Performance [Full-spec emulator][E1][E20]
Measure Coverage [Simulator]
Set an Action into Programs
Manage Events
Use Hook Function
About Input Value
Exclusive Control Checking Tool
Pseudo-error Debugging [Full-spec emulator][E1][E20]
Debugging CAN Bus Reception Procedures [Full-spec emulator][E1][E20]
Measuring CAN Bus Reception Processing Times [E2]
WINDOW REFERENCE
COPYRIGHT