Everything
2.4.2 Disconnect from the debug tool

By clicking the button on the Debug toolbar, CS+ cuts off the communication with the connected debug tool.

After disconnecting from the debug tool, the Statusbar of the Main window changes as follows:

Figure 2.62

Statusbar Indicating Disconnection from Debug Tool

Caution

The debug tool cannot be disconnected from CS+ while the program is running.

Remark

Disconnecting the debug tool will close all the panels and dialog boxes that can be displayed only during the connection.