Everything
Everything
top
Debug Tool
FUNCTIONS
Measure Execution Time of Programs
2.12
Measure Execution Time of Programs
This section describes how to measure the execution time of the program.
Differences Information
Previous Topic
Save the contents of execution history
Next Topic
Configure the timer operation
Table of Contents
Overview
Preparation before Debugging
Configuration of Operating Environment of the Debug Tool
Connect to/Disconnect from the Debug Tool
Download/Upload Programs
Display/Change Programs
Execute Programs
Stop Programs (Break)
Display/Change the Memory, Register and Variable
Display Information on Function Call from Stack
Collect Execution History of Programs
Measure Execution Time of Programs
Configure the timer operation
Measure execution time until stop of the execution
Measure execution time in a section [IECUBE][Simulator]
Measurable time ranges
Measure Coverage [IECUBE][Simulator]
Set an Action into Programs
Manage Events
Use Hook Function
Measuring Current Consumption [E2][Simulator]
Use the Simulator GUI [Simulator]
About Input Value