Everything
2.15.2 Display only particular event types

Click on the toolbar button to display only the particular event type.

 

Displays events related to the Hardware Break.

 

(except [Simulator])

Displays events related to the Software Break.

 

Displays events related to the traceNote.

 

[IECUBE][Simulator]

Displays events related to the timer.

 

Displays events related to the action event (Printf event).

 

Displays the built-in events (Unconditional Trace event and Run-Break Timer event).

Note

[E1][E20][EZ Emulator]
This button is available only when the selected microcontroller incorporates the OCD trace function.