Everything
2.15.4.3 Edit combination conditions of events [E1] [E20]

Edit the combination condition for a combination break event comprised of multiple events set.

 

Caution

This function is enabled only when the selected microcontroller supports combination break events.

 

Perform this operation in the Combination Condition dialog box [E1][E20] that is opened by selecting [Edit Condition...] from the context menu after moving the caret to a combination break event you want to edit on the Events panel.

Figure 2.159

Example of Combination Condition Dialog Box

(1)

Editing [Combination] area

Select the combination condition from the following drop-down list.

OR

The condition is satisfied when one of the set events is encountered (default).

Sequential

The condition is satisfied when the set events are encountered in the specified sequence.

Caution

When [OR] is selected, up to two break events can be specified.
When [Sequential] is selected, break event can be specified for the 1st to the 2nd position.

(2)

Editing [Object event] area

This area displays details on the break event set as a combination break event.

When [Sequential] is specified in the [Combination] area, the order of display here corresponds to the order in which the conditions are to be satisfied. To change the order, select a target event and click on the [Up] or [Down] buttons.

(3)

Editing [Reset event] area

Reset events are always enabled.