Setting the Printf event as one of action events allows you to output the value of the specified variable expression to the Output panel. This can be done by executing a printf command after temporarily stopping the program at an arbitrary position.
To use this function, follow the steps below.
2.16.1.3 Check the output result
Also see "2.17.7 Points to note regarding event setting" for details on Printf event settings, including the allowable number of valid events.  | 
 / 
 / 
) or execution ignoring break-related events (
).