Connect a host machine and E1. If required, connect a target board, too.
You can make a choice between FINE communications [E1(Serial)] and JTAG communications [E1(JTAG)] as the communication method to the target system (see "2.3.1 Select the debug tool to use").
See E1 User's Manual for details on the connection method.