The form in which the data in the [Value] area is displayed can be freely changed using the toolbar buttons shown below.
| Shows the following buttons that change the form in which values are displayed. | ||
| Displays the value of a selected watch-expression in per-variable predetermined notation (default) (see "Table A.11 Display Form of Watch-expressions (Default)"). | ||
| Displays a selected item in Float. However, this is valid only when the selected watch-expression consists of 4-byte data. | ||
| Displays a selected item in Double. However, this is valid only when the selected watch-expression consists of 8-byte data. | ||
| Adds a hexadecimal equivalent for the displayed value of a selected item at the end of the value, with the equivalent enclosed in parentheses ( ). However, this information is not added when values are displayed in hexadecimal. | ||
 AutoSelect
AutoSelect Hexadecimal
Hexadecimal Signed Decimal
Signed Decimal Unsigned Decimal
Unsigned Decimal Octal
Octal Binary
Binary ASCII
ASCII Float
Float Double
Double