The following are the editor features provided by CS+.
Caution  | C++ source files are only supported by CC-RX.   | 
 
 
-  | Display and editing of the contents of files 
The contents of text files and C/C++ source files can be displayed/edited. 
  | 
 
-  | Support of the code outlining 
For a C/C++ source file, this function allows you to expand and collapse source code blocks so that you can concentrate on the areas of code which you are currently modifying or debugging.  
  | 
 
-  | Mixed display of C/C++ source text and disassembled text 
By connecting to the debug tool, the C/C++ source text and the disassembled text can be displayed together on the same panel. 
  | 
 
-  | Source level debugging and instruction level debugging 
By connecting to the debug tool, the C/C++ source file can be debugged either at the source or the instruction level. 
  | 
 
-  | Display of the code coverage measurement result 
By connecting to the debug tool that supports the coverage function, the code coverage measurement result can be displayed.  |