1.3.1 RI78V4 V2.xx.xx
The kernel, which is the processing block that forms the core of the RI78V4 V2.xx.xx and the main processing block for the service calls provided by the RI78V4, provides the following functions.
To support various execution environments, the RI78V4 V2.xx.xx extracts hardware-dependent processing that is required to execute processing as user-own coding modules, and provides it as sample source files. This enhances portability for various execution environments and facilitates customization as well.
Remark For interrupt handlers written by C language(defined the attribution "TA_HLNG" in interrupt handler definition "DEF_INH" in system configuration file), the user is not required to write the relevant interrupt entry processing because the C compiler automatically outputs the interrupt entry processing corresponding to the interrupt request name.