Everything

Generating code

5. Generating code

When the configuration of the functions to be used is completed, generate the program.

 

The program is generated by clicking the [Generate Code] button on the toolbar.

The generated program is displayed in the Project Tree.

 

Tip

Before generating code

You can confirm the content of the program that will be generated without actually generating the code. This is called a "Code Preview" function. Try this function by selecting [Code Generator Preview] from the [View] menu. "Code Preview" is sometimes shown by the kind of microcontroller in the Project Tree.