This tab is used to set the build tool and debug tool plug-ins to be read in when this product is started.
Caution  | We recommend that the check box for the plug-in for the microcontroller that is the target for development is not deselected. 
Deselect the check boxes for the build tool and debug tool plug-ins that are for microcontrollers that are not the target for development. For example, if only the plug-in for the build tool is deselected, the file to be downloaded by the debug tool will not be found and an error will occur.  | 
 
Figure A.55  | Plug-in Manager Dialog Box: [Basic Function] Tab  | 
 
 
The following items are explained here.
[How to open]
-  | From the [Tool] menu, select [Plug-in Setting...].  | 
 
[Description of each area]
This area shows a list of the build tool and debug tool plug-ins installed in this product, in the following format.
| 
 
Module Name 
 | 
 
Shows the plug-in module names. 
The plug-ins read in when this product is started are selected with check boxes. 
 | 
| 
 
Description 
 | 
 
Shows a simple description of the plug-in. 
 | 
 
[Function buttons]
| 
 | 
 | 
| 
 
OK 
 | 
 
Applies all setting and closes this dialog box. 
 | 
| 
 
Cancel 
 | 
 
Cancels the designated condition and closes the dialog box. 
 | 
| 
 
Help 
 | 
 
Displays the help of this dialog box. 
 |