Below are input conventions for configuring information in the panels and dialog boxes provided by CS+.
The following character sets are allowed for input.
| 
Table D.1 | List of Character Sets | 
|  |  | 
| 
ASCII | 
Single-byte numbers, letters, and punctuation | 
| 
Shift-JIS | 
Double-byte letters, numbers, punctuation, Hiragana, Katakana, and Kanji, and single-byte Katakana | 
| 
EUC-JP | 
Double-byte letters, numbers, punctuation, Hiragana, Katakana, and Kanji, and single-byte Katakana | 
| 
UTF-8 | 
Double-byte letters, numbers, punctuation, Hiragana, Katakana, and Kanji (including Chinese), and single-byte Katakana | 
Numbers may be input in the following base formats.
| 
Table D.2 | List of Number Bases | 
|  |  | 
| 
Decimal number | 
Starts with 1 to 9, followed by a sequence of the digits 0 to 9, and 0 | 
| 
Hexadecimal number | 
Starts with 0x, followed by a sequence of the digits 0 to 9 and the letters a to f 
(As for capital letter/small letter of the alphabet, it is pretermission.) |