Display the variable information (variable name, file name, attribute, read count, write count, data coverage, etc.) in the program.
The latest variable information that can currently be displayed (see "1.1.2 Types of analysis information") is displayed on the following Variable List panel, which is opened by clicking the
button on the Main window's toolbar.
Note, however, that the variable information in the files not to be analyzed is not displayed in this panel (see "1.1.1 What is analyzed").
See the Variable List panel for details on each of the variable information items displayed.
[E20[RX]] |
[CC-RX] |
The display contents are updated each time program execution is stopped. |
The value of the information that has been changed because of the execution of a program is shown highlighted (the color depends on the configuration in the [General - Font and Color] category of the Option dialog box). To reset the highlighting, click the |
The current row mark ( |
Information for functions defined outside the active project, and which are never referenced from the active project, is ordinary not displayed in the Variable List panel. |
button on the toolbar.
) indicates the current row.