|
Update I/O header file on build
|
Select whether to update the I/O header file at build.
The I/O header file is updated when the device file is newer than that at generation of the I/O header file or properties related to generation of the I/O header file have been updated. Update is performed by automatic overwriting and a backup file with the bak extension is created.
This contents are common to all the build modes.
|
|
Default
|
No
|
|
How to change
|
Select from the drop-down list.
|
|
Restriction
|
Yes(Checking the device file)
|
Updates the I/O header file when the device file has been updated at build.
|
|
Yes(Checking the property)
|
Updates the I/O header file when the properties have been updated at build.
|
|
Yes(Checking the device file and the property)
|
Updates the I/O header file when the device file or properties have been updated at build.
|
|
No
|
Does not update the I/O header file at build.
|
|
Device file on generating I/O header file
|
The file name and version of the device file when the I/O header file was generated are displayed.
Note that this property is displayed only when a choice other than [No] was made in the [Update I/O header file on build] property.
|
|
Default
|
The file name and version of the device file when the I/O header file was generated
|
|
How to change
|
Changes not allowed
|
|
Current device file
|
The file name and version of the device file which is installed in the running CS+ environment are displayed.
Note that this property is displayed only when a choice other than [No] was made in the [Update I/O header file on build] property.
|
|
Default
|
Current device file
|
|
How to change
|
Changes not allowed
|
|
Output 1bit access
|
Select whether to output the 1-bit macro definition for IOR access in the I/O header file.
This contents are common to all the build modes.
|
|
Default
|
Yes
|
|
How to change
|
Select from the drop-down list.
|
|
Restriction
|
Yes
|
Outputs 1-bit access.
|
|
No
|
Does not output 1-bit access.
|
|
Enable MISRA-C option
|
Select whether to output an I/O header file compatible with the MISRA-C rules.
This contents are common to all the build modes.
|
|
Default
|
No
|
|
How to change
|
Select from the drop-down list.
|
|
Restriction
|
Yes(-misra_c=on)
|
Outputs an I/O header file compatible with the MISRA-C rules.
|
|
No
|
The MISRA-C rules are not considered.
|
|
Output macro definition of device file name
|
Select whether to output the following macro definition (macro indicating the target CPU) that is treated as predefined macro names in CA78K0R.
#define Macro of device file name 1
|
|
Default
|
No
|
|
How to change
|
Select from the drop-down list.
|
|
Restriction
|
Yes(-ca78k0r=on)
|
Outputs the macro definition of the device file name.
|
|
No
|
Does not output the macro definition of the device file name.
|