This dialog box is used to select the predefined macros to disable and set it to the area that this dialog box is called from.

The following items are explained here.
On the Property panel, select the following properties, and then click the [...] button. |
From the [Compile Options] tab, [Invalidates the predefined macro] in the [Source] category. |
From the [Individual Compile Options(C)] tab, [Invalidates the predefined macro] in the [Source] category. |
From the [Individual Compile Options(C++)] tab, [Invalidates the predefined macro] in the [Source] category. |
The list of the predefined macros which can be disabled for the area that this dialog box is called from is displayed.
Select the predefined macros to disable to set to the area that opened this dialog box, via check boxes.
In the area that opened this dialog box, if a predefined macros to disable is already set, the check box for that macro will be selected by default. |