Everything
2.9 Set Library Generate Options

To set options for the library generator, select the Build tool node on the project tree and select the [Library Generate Options] tab on the Property panel.

You can set the various create library options by setting the necessary properties in this tab.

Caution

This tab is not displayed for the library project.