Sets the analog voltage output to the ANOn pin.
[Syntax]
#include “r_cg_macrodriver.h”
void R_DACn_Set_ConversionValue ( uint8_t reg_value );
Remark n is the channel number.
[Argument(s)]
| I/O | Argument | Description | 
| I | Uint8_t reg_value; | D/A conversion value (0x0 to 0xFF) | 
[Return value]
None.