R_KB2m_TKBOn1_Forced_Output_Stop_Function1_Start
 
Starts forced output stop function 2 
for timer output TKBOn1.
 
[Syntax]
void   
R_KB2m_TKBOn1_Forced_Ourput_Stop_Function1_Start ( void 
);
 
Remark         
m is the unit number, and n is the channel number.
 
[Argument(s)]
None.
 
[Return 
value]
None.